Hello,
there is the following issue:
- TPS56121 (5V -> 3.3V & 5V -> 1.2V)
- Type III amplifier compensation
- result of Compensation Calculator Tool (Rev. D) does NOT correspond to the measured results at all
- in the forum I found a similar problem: "Type III Voltage Mode Compensation Software Tool" from Bill Drumheller
The theory for the factor k_Venable is getting this factor from a required phase boost.
The tool should place zeros near or below the double pole that is created by the inductor and output capacitors.
But it places them above the double pole.
Also for type III amplifier compensation it should be:
- zero_of_compensation * sqrt(k_Venable) = f_crossover
- f_crossover * sqrt(k_Venable) = double_pole_of_compensation
But tool shows a factor of k_Venable and NOT the square-root of k_Venable; this would be suitable for Type II amplifier compensation!
Maybe this behaviour is due to the fact that it is an EXCEL-sheet for various DC/DC-converter-ICs.
For not to use trial&error method I did "Manually enter P's and Z's" and chose Fco:
- zeros @ double_pole
- from that and Fco I get k_Venable
- Fco and k_Venable results in P's
- then I used the calculated values for the compensation
=> now bode-plot and calculated values for Fco and phase-margin correlate much better
but there is still little correlation between 'Compensation Calculator Tool' and measurement.
Is there any plan to revise that EXCEL-sheet for to get results that are comparable to measurements?
Many thanks
regards
Udo Weik