I would like to confirm absolute maximum rating for transient input of LM26001/26003-Q1.
For anutomotive application, customers need to consider transient input voltage (for load dump).
In the datasheet, there is not it and is input voltage 40V DC.
If you have, could you please provide the data or the information of transient input?
Best regards,
Atsushi Yamauchi