Hi,
I have used R1 = 1M ohm, R2 = 270K ohm. So according to equation (3) in the datasheet of TPS61032, if my input voltage/VBAT is 2.35V or below it then the LBO should go low... But this does not happen and the LBO pin remains active high all the time. Please suggest what to do asap...
Regards
Kamesh Lakhwani