Hi,
I purchased the TPS63020EVM evaluation module (EVM) because the ti TPS6302x data sheet states this device can provide a power
supply 3-A Output current at 3.3V in Step down mode (Vin=3.6V to 5.5V). I tried testing this EVM to determine the module's behaviour under a one (1) Amp load and the EVM could not provide 1 amp continuously.
I'm sure if I used the correct method. I added a 3.3ohm 5watt resistor to the output in order to draw 1 amp continuously, but the EVM brings down the 3.3 Vout to 2V, and also notice the input was at 2V. I used a 5Volt, 3amp power suppy to provide the input of 5VDC.
The goal is to power a 3.3 V device that draws 1 to 1.5 amps of current with the EVM.
What is the proper method for load testing this EVM for my scenario?
Regards