Hello,
I am designing a circuit with the TPS63060 buck/boost IC. The input voltage is 4 alkaline batteries (3.6V to 6.4V) with the output set to 6V. The Typical Application schematic in the datasheet shows a 1uH Coilcraft XFL4020-102 inductor. This part costs about $1.50. I am trying to find a lower cost inductor. I found a Taiyo Yuden NR3015T1R0N inductor that has a max DCR value of 36 mOhms. The Coilcraft part has a DCR value of 12 mOhms. Are there any concerns with using the Taiyo Yuden inductor in this circuit?
Thank you,
Randy