I am using the TPS63030 for a buck-boost operation from a Li-ion battery. Out put is set to 3.1V (approximate) using a 1.5M and 280k resistor divider. My inductor is a 1.5uH (XFL4020-152meb) from coil craft. I have a 47uF electrolytic on the input in parallel with a 10uF ceramic. On the output I have 2x10uF ceramic caps with a 470uF Electrolytic. My VINA and Ven and Vsync are all tied together with a 0.1uF cap. I have the ground on that cap and the resistor divider isolated from the power ground as is shown in the data sheet.
My output voltage is correct and remains stable, however, my current draw at no load is 3.6mA. where the data sheet shows it should be about 25uA which is what I need. Is there something I'm missing to get the current draw down to micro-amp range?
Thank you!