I want to design a voltage converter from 24V to a variable output voltage from 12V to 36V with I(load)= 500mA.
Actually, I'm planning to use SEPIC topology.
I'm thinking of using the LM5000 (Imax=2A),
but in the datasheet, there is no remark for SEPIC topology.
1) Is the LM5000 suitable to be used in SEPIC topology?
2) Are there any Spice Models of the LM5000?
Best regards, Andy