Hello Team,
Please tell us how to use WEBENCH and Excel tool.
-> Excel tool : TPS4306x_BOOST_CALCTOOL_REVB.xls
It is an error to run under the following conditions by WEBENCH.
1) In TPS43060,
What is the reason circuit calculator can't create design?
2) In Case1 and Case2 of TPS43061,
Why the result is different?
Case 1 is the larger input current than Case 2.
3) Is circuit can be realized in the following Case?
4) It is not an error to run under the following conditions by Excel tool.
And, specs of recommended FET is not output.
Please tell us how to use Excel tool.
<Case 1>
Vin : 9.6 to 12.6V
Vout : 24V
Iout : 10A
[Result]
TPS43060 : Circuit Calculator can't create design
TPS43061 : Can't find suitable FET for the design
<Case 2>
Vin : 12.8 to 16.8V
Vout : 24V
Iout : 10A
[Result]
TPS43060 : Circuit Calculator can't create design
TPS43061 : Current exceeds limit
<Case 3>
Vin : 16 to 21V
Vout : 24V
Iout : 20A
[Result]
TPS43060 : Circuit Calculator can't create design.
TPS43061 : Can't find suitable FET for the design
Best regards,
Kato