Respected Sir,
This is Gaurav Kothari From UK Electro Mech Systems, Mumbai, India.
We are in manufacturing of Electronic Lockers. We are basically using a microcontroller with voltage range of 4.5 to 5.5 volt. but the supply voltage we have is from LI-Polymer battery which come in range of 3.0V to 4.2V. So i such case we are planning to use TPS-61032 - 5V Step up Booster IC.
We need your guidelines to clear out some confusion we are facing in designing the circuit.
The IC we are using is TPS-61032 16 pin PWP package.
There are 3 PGND pins (Pin 3,4,5) and a different GND pin (PIN 11). What the difference between this PGND pins and GND pins. can i connect this both pins together with also thermal pad.
and also please let me know how can i program the LBI pin as if i need to alarm the signal when the battery voltage reaches 3.0V. what value resistor should be placed at pin LBI to make LBO pin Low.
can i place a LED at LBO pin using a transistor for low battery indication.