Other Parts Discussed in Thread: TPS54519,
Hello Team,
We are using TPS54719 device to generate 2.5V@5.91A using 3.3V as input. Attached is the spreadsheet where I had calculated the Vout min and max for 2 devices(TPS54519 and TPS54719) in 4 cases (1.8V@1.36A, 1.35V@3.66A, 1V@4.84A, 2.5V@5.91A using 3.3V as input +/-5% tolerance) . I am getting Vout min as 2.668V and Voutmax as 2.464V when Vout is 2.5V. Please review this and suggest how to correct the design. 3034.G450_TPS54519-719 _Vout_calc.xlsx