Hi all
Would you mind if we ask TPS54332?
<Question1>
Is there the sequence between Vin and Enable(1.25V)?(At the first, Vin needs to be overt UVLO?)
Especially, after Vin is over UVLO threshold level(3.5V), Enable voltage require to be over 1.25V(typ).
Is our recognition correct?
<Question2>
On the datasheet P11, there is the description "TI recommends using an external VIN UVLO to add Hysteresis unless VIN is greater than (VOUT + 2 V)".
So, unless we use external Vin for Enable, we don't need to keep VIN is greater than (VOUT + 2V), do we?
Our customer uses following condition;
It is no problem, right?
-Condition-
Vin=5V, Vout=3.3V/No Load
We confirmed with above condition, as the result, it didn't output normally like as attachment file.
CH1 : Vin, CH2 : Enable pin, CH3 : SW pin
And then, we tried with Vin=5.3V(Vout3.3V+2.0V), SW operated normally.
Furthermore, when we use internal pull-up about Enable pin, it rewquire to keep that VIN is greater than (VOUT + 2V), doesn't it?
Kind regards,
Hirotaka Matsumoto