I used this chip in a past design in a boost configuration using the recommended values and schematic from WEBENCH. It creates an 11V output from a 7.4V battery. This worked fine using an IRFR3707ZTRPBF and STD35NF3LLT4 as the MOSFET devices. So now we are making a variation of the part and the output goes to 12V and the output current is much less. So we changed the mosfets to AO3400A.
The new design will only occasionally (like every few seconds) momentarily jump to 12V but then immediately discharges back to battery voltage (following the output capacitor discharge) and the output basically follows battery voltage.
Can this MOSFET change actually be causing this behavior or is there something else we are missing? We cannot find any other changes.