Other Parts Discussed in Thread: LM5170-Q1, LM5170
Hi,
I am using a LM5170-Q1 EVM, to control the bidirectional power flow between two battery packs. The high voltage (HV) side is 48V, and the low voltage (LV) side 20V.
I am not sure how to determine the maximum load current at the LV side? and what are the limiting factors for this maximum current?
I learned from the use guide that the maximum power is around 700W when HV = 48V and LV = 12V. Does this power limit apply to different HV and LV combinations?
Many thanks.