Hi,
Please tell me about the setting value at startup and the behavior of IDAC_current.
· If the VIDS goes from "L" to "H" after EN (Enable) at startup, will the initial value of VID [5: 0] be reflected?
What is the initial value of VID [5: 0]? (The upper 3 BIT is the VIDA - C terminal, and the lower 3 BIT is the initial value?)
What is the current value of IDAC_OUT at each of the following timings?
* When only VDD is input (EN: Disable): Vout at 0 uA?
* For VDD + Enable: Vout set with current value of Rset?
Best Regards,
Yuto Sakai