Hello,
The formula for the output voltage is different in the datasheet and EVM User Guide (please see images below)
Datasheet:
EVM User Guide
Please confirm which formula is correct.
In our application we've used the matching formulas (due to the EVM user guide and the WeBench calculations) for both positive and negative outputs, however the outputs are not closely matching. I'm seeing <1% tolerance on the positive voltage rail whereas I get <4% on the negative rail. Please advise on this issue.
Thank you.