Hi I am using TPS40170 regulator to convert 16V to 32 V range input to 3.3V output,4A circuit. with the initial design some boards are functional at all input ranges ,but some boards are not functional at 16V at room temperature and -40C.
I'm using 10nf soft start capacitor and when I changed Css to 47nf all boards are functional at all cases . With 10nf soft start capacitor I have seen a weird behavior with this supply, at 16V module will not turn on , but it is functional at 8V and 24V at all temperature ranges.