Hi,
We got a question from the customer about LM5161-Q1.
Could you help us?
[Question]
How much is the variation of the constant 1.008*10^(-10) under the following condition?
Topology: Inverting Buck-Boost
Vin: 6~32V, 6~20V
Vout: 8V
They are concerned about reaching the current limit due to the variation of ton. Therefore they need this to estimate ton.
Best Regards,
tateo