Other Parts Discussed in Thread: LMV358
Hello, I have a circuit here with the LM73606. The problem is that I have a very large voltage change when load changes. I have set the voltage to 15V, I have this voltage charged with 3.8A. On the capacitor C155 I have a voltage change of 188mV. I think this voltage change is too big. At higher currents, the voltage change increases even further. At the moment, I have no idea how to get there. The problem with the circuit is the wide output voltage range of 4.5 to 23V.
Is there any other circuits for which the step size does not change over the setting range? Over the 256 steps, the step size changes from 20mV to 450mV. I would appreciate constructive suggestions.
The coil is a Coilcraft XAL1010-682MED.