Hello,
I am having a problem with my TPS65721 PMU on my own custom board not charging my 3.7V 500mAh Li-po battery. I have tried 3 different RIset values at 1k, 1.5k, and 3.3k and see no difference. The charge current is measuring in the micro-amps and will only charge the battery about 100mV if left charging overnight. I have reviewed my schematic and layout and do not see any issues. I have tested multiple batteries to ensure that it is not my battery causing the problem.
I am also having a problem where the PMU will not shut down DCDC or LDO. In attempt to turn the LDO and DCDC regulators off, after PB_IN is released high, HOLD_DCDC1 and HOLD_LDO1pins are pulled low. When this happens, the DCDC regulator drops from 3.3V to 1.8V and the LDO drops from 1.8V to 0.6V. I am under the impression that the voltages should both be at 0V.
Let me know if anyone has experienced the same issues.
Regards,
-James