I am trying to cause a AM335x system reboot from the SYSCONFIG peripheral after a software controlled shutdown (OFF=1 and POWER_EN=0). Using the AM335x RTC is not an option. I have 5.5V tied to the TPS65217B's AC input and a TPS76950 5V regulator tied to the USB input. The TPS76950 is enabled when LDO_PGOOD goes low at shutdown. The circuit functions as predicted but does not wake the TPS75217B even though the circuit meet the risetime requirements. Is there a delay period between the time LDO_PGOOD goes low and the wakeup (AC↑,USB↑,PB↓) conditions are sampled?