Gentlemen,
Can you please help me determine how to properly configure the TPS65217 for my Battery Free configuration? Here are some details of my design.
- We are using an AM3358 processor with the TPS65217D PMIC, but we do not require system battery operation. We do have a requirement to keep time/ date persistent, but do not want to make the whole system battery powered for this. I have added an external Real Time Clock Module with a coin cell to allow my system to keep track of time for up to a year with no AC power Connection. This part of my design works as intended. The coin cell has its own trickle charger and does not use the PMIC battery charger.
- My design has a 5V bias supply available anytime AC power is available. The Bias voltage has a capacity of about 0.5A.
- My design has another 5V system power supply available at much higher currents that is only available when the system power is turned ON.
- My initial inclination was to connect the 5V bias voltage to the USB input of the PMIC and the other 5V power to the AC Power input with the Battery terminals floating. The design intent was for the bias voltage to keep the PMIC powered anytime AC power is available, but to switch over to the higher current supply when the system is turned ON. The problem with this configuration is that the PWR_EN signal gets activated when the system is first plugged in (bias voltage turns ON) which causes the system to turn ON without the power switch button press.
- Another configuration I have tried is to connect 5V bias to the Battery Input. In this configuration, the PMIC behaves as intended - ie it does not cause the PWR_EN signal to activate until the Power Button is pressed (PMIC PB input). The issue with this configuration is that the PMIC ends up drawing all of the power (about 0.4A) from the Bias Supply even after the higher power 5V supply is available at the PMIC AC Power input.
So, I would like TI's help to figure out how to get the PMIC to use our high power 5V power rail when it is available and only use our 5V bias supply when the higher power supply is not available (with no battery). If this is not feasible, then I will end up adding a power switch upstream of the PMIC to manage the transition from 5V bias supply to 5V system power supply. It seems like the PMIC should be able to manage the two 5V power supplies, but it is not clear how this should be done.
Sincerely,
Randy Holmberg