Hi.
I read an article: "Powering the TMS320C6745 and TMS320C6747 with the TPS650061" and I don't understand why are using the precision resistors:
R2 - 47.5k
R7 - 475k
R9 - 47.5k
Can I use this option ?
R2 - 47k - 5%
R7 - 470k - 5%
R9 - 47k- 5%
On Figure2. TPS650061 Schematic Diagram - pin 1 (MR) directly connected to the VODC (1.2V). I want to use this pin for manual reset.
For this i must be connected MR-pin with button through the resistor to the VODC (1.2V) or to the VIN(5V) ?
Pull up resistor must be 470k or 47k ?