Hello,
I need to add a significant amount of capacitance to the SYS output pin of the TPS65217C because it's needed to ensure a correct power down sequence when the 5V inputs are suddenly removed (no battery application). See previous post for more details about this: https://mail.google.com/mail/u/0/#inbox/14d531d2f37444bc
I'm adding around 1000uF (a little less) to the SYS pin, and I want to know if the PMIC will be OK or it's too much peak power through the internal switches.
Thanks,
Max