Hi,
We are designing with the TPS65217C and the Sitara AM3352. Our system has two power sources coming from different supplies, Primary +5V and Secondary +5V. In reading the datasheet for the TPS65217 (Revised January 2015) it is not clear to me if I can use this device for the following use case.
Run the primary +5V to the AC input pin and run the secondary (Backup) +5V to the BAT pin. We would need the system power to be applied if EITHER OR BOTH of the +5V souces (Primary or secondary) is on.
Our voltage outputs use case will be default as described in the device comparison table on page three of the datasheet for the TPS65217C device.
My concern comes from the note on page 76 (Table 36 use case 3 for "Output Rail Status on initial power connection") of the TPS65217 datasheet statement that LDO1 is off when BAT is connected to 5V supply and that PB_IN must be pulled low to enter the [WAIT PWR_EN] state. This might be a problem for us if the primary power is off, and we try to apply power via the backup slave unit on the BAT pin. We have no power switch, and the system must come up autonomously when plugged in. Is there a solution where we can cold boot from either power source without pushing a button using the TPS65217C?
Will appreciate any feedback and help on this. Thanks in advance.