Other Parts Discussed in Thread: TPS65381-Q1
Dear Specialists,
My customer is considering TPS65381-Q1 and has a question.
I would be grateful if you could advise.
---
When the IGN_PWRL of the normal operation register is set to 1 in the device,
if an abnormality occurs and transition to Stanby mode,
It will not return from Stanby mode unless the IGN terminal goes from Low to High.
Is it correct?
Also, the voltage to recognize that the IGN pin input, What voltage is Low and High?
---
I appreciate your great help in advance.
Best regards,
Shinichi