Hello, my question is regarding a non-rechargeable lithium coin cell used as the backup battery for the TPS65930. My product is currently undergoing IEC 60601 testing and the examiners have indicated that there should be a diode between the coin cell and the TPS65930 device to prevent current flowing back in to the battery.
I have no problem adding a schottky diode, but I wondered if there some features of the TPS65930 that deem this unnecessary, and save me from updating the circuit board, again.
Thank you.