Q: Can HFCLK be turned OFF when the PMIC is in ACTIVE mode?
A: Yes, HFCLK can be switched OFF when PMIC in ACTIVE mode.
Side effects/Concerns -
- Cannot access internal registers as the OCP clk is not generated.
- Cannot use MADC functionality as the MADC_CLK is not generated.
- PWM0 and PWM1 blocks are clocked by 32K generated from HFCLK, this functinality will also not work.