Hi,
As per appnote SLVA163, I would like to protect a 12V input but the issue I have is that my 12V input is a battery so mA's of current are critical. Your appnote indicates using low-value resistors like 2.49Kohms which would result in high current draw. How much could I increase the value of R1 and R2 to the point where the TPS2400 circuit would not respond quickly enough ? R1 and R2 turn on/off the base of a MMBT5551 transistor which in turn feeds Vin of the TPS2400.
Thanks,
-Steve