I have a problem where my LM5069 fails shorted, Vin to Gnd.
I am using this as an inrush control for the front end of a power supply. I am not measuring input current, I am just using it as a charge pump to ramp up and saturate a pass FET.
Sometimes, after an inrush event, the fails short. The FET does not fail. Replace the IC and it all works as expected.
My testing is being done at 60VDC input. I have a large 60V power source, I quickly connect the power source to my power supply input and monitor inrush with a current probe. Then I disconnect the power source by pulling the wire off the terminals. I think this is a good representation of a hot swap input.
I do have a 100 ohm resistor from Vin to drain of the pass FET, and a 68V zener from Vini to ground. This is to protect from input transients