Hi all,
Would you mind if we ask about TPS25940?
Our customer would like to use the range of ILim from 0.5A to 5.2A.
The datasheet shows the ILim(A) which is possible to adjust from 0.6A to 5.2A using extenal resistance.
On the other hand, the datasheet also shows "R (ILIM) = OPEN, Open resistor current limit (Single Point Failure Test: UL60950).
If we'd like to set the ILim 0.5A, is it possible to us "R (ILIM) = OPEN"?
Or, is it abnormal function to use normal situation, isn't it?
Kind regards,
Hirotaka Matsumoto