Application : linear - 28V 6A continuous DC,
Purpose : load protection from UVLO, OV and di/dt & SC.
The power limit set point from calculation (SPREAD SHEET) SLVC033 is set at 84W, while power supply power limit is 168W (APLLICATION LIMIT - 28*6 = 168).
1- THE POWER LIMIT CURVE FORMED IN THE SPREAD SHEET SEEMS TO LIMIT THE VOLTAGE AT 15V,
2- WILL THE DEVICE WORK PROPERLY AT FULL LOAD OF 28V WHEN PLIM IS SET AT 85W ??