Hi, here are my specifications:
VIN: 24V (batteries)
VOUT: No control of the load (RES./CAP./IND.) maximum output current 30A continuous.
The actual current limit is 184A for 2msec.
Mos: 2x IRFS7534
- If the switch is activated and the mosfet is full ON, then a capacitive load is apply (34000uF), the output is able to charge the capacitors without a fault condition. (current threshold is high enough
- If the switch is activated and the mosfet is full ON, then a short is apply (VOUT = GND), the mosfet is able to turn-off within the SOA limit.
- If a short is apply at the output then ENABLE is activated, how is it possible to protect the MOSFET ?
Is there any circuit that can be added to meet this requirement ?