Hi,
I have let the reference design found in www.ti.com/.../tps2375-1.pdf (page 1) made as part of a PoE application. Triple-checked everything, but this part doesn't work.
Even the detection phase goes wrong: when I manually begin to add voltage between the "~" pins of any of the two bridge rectificiers, the circuit begins to consume a lot of current (10mA @ 2V and 0.5A @ 2.7V and exponentially growing (didn't dare to go above 1A)).
Does anyone have an idea, what could go wrong?
Thanks,
Gergely