Hi Team,
Our customer are evaluating the ORing circuit at the following conditions.
[Conditions]
-Battery1 = 7.6V
-Battery2 = 7.58V
-J4 & J9 = High
-Other jumper is default
-R9 remove
- 270kohm is connected to parallel to R20
However, they were confronted with the following problem.
Could you please let us know if you have any solution?
[Problem]
"Battery1" is charged when “Battery1=7.6V” and “Battery2=7.58V”.
However, they would like to prevent this phenomenon.
I believe that we can solve this problem if we use this device with the Non-ideal Diode mode.
So, we have to connect "Pin1_CTRL-1" and "VIN1" of Jumper6.
Is my understanding correct?
And, I have one more question.
I believe that “DEVSLP pin” is “DMODE pin”.
why are mention contents different from the datasheet?
Regards,
Kanemaru