Hi,
My customer has questions about LM5060-Q1.
Could you tell me about questoins?
[Question]
My customer considers design of LM5060-Q1. He has some questions from datasheet.
- What is the purpose of changing Itimerl(6uA) to Itimerh(11uA) in start up time?
- Is there any shutdown sequencing requirement?
- How much is the value of EN pin input impedance?
- Could you tell us the internal charge pump circuit and fsw of charge pump?
My customer consider VIN bypass capacitor.
He want to know about frequency of ripple and noise from chrge pump circuit.
- In reverse current event, my customer should care of OUT pin and SENSE pin reverse current limit.
Datasheet show us OUT pin reverse current is 4mA max and SENSE pin reverse current is 25mA.
Is these value's condition including over temperature?
- Datasheet recommend Figure 34 at if the output load is highly capacitive.
Why does the D5 and D7 is needed to protect internal diode? What is the path of this current flow?
- The OUT pin reverse current limit is 25mA. Why is 25mA?
What does the internal circuit be related?
And in figure 34, what do you recommend If-Vf characteristic of D5?
- In figure 34, how is the method of R1 protect the GATE pin from reverse current exceeding 25mA?
Best Regards,
tateo