I am using the LM25066 device and a 1m-ohm sense resistor. When I use the default values listed in Table 41 of the device specification (CL=GND), I have readings that are roughly 35% low. I have taken several measurements between 1A and 11A.
The section about Determining Telemetry Coefficients Empirically with Linear Fit implies that there might be some slight variation, but 35% does not seem slight to me.
I have verified the voltage at the LM25066 input pins are very close to the voltage drop over the sense resistor.
If I determine the coefficients empirically with linear fit (as described in the doc), I get very different coefficients than the defaults.
I am curious what the expected variation is, and what might be causing this issue.