I am in the process of designing a PoE injector that supports 802.3af, at and also higher power over 4 pairs. I am currently using a TPS23861 in auto mode with no I2C interface connected. Everything appears to work fine with the af and at PDs we have tested. I realize the there are several high power implementations commercially, but in the absence of 802.3bt there is no real standard. We currently have a Hikvision DS-2DF8836IV-AELW 60W PTZ camera as the PD. I am told that it works with a Suplet LAS60-57CN-RJ45, but have been unable to obtain enough detailed information to go straight to a working design.
I have tried using 2 ports connecting one pair to each, and 1 port connecting both pairs to it. The former does not seem to work even on af and at PDs. Looking at "VPORT" it seems that detection fails. The latter runs all af and at PDs we have tested. With the 60W camera it succeeds at detection, does a 2 event classification, and turns on, only to turn off again presumably because the current exceeds ICUT.
Do you by any chance have some insight into what I might be able to do to resolve this. Many thanks for your help.