Hi E2e,
Our customer has a question concerning the TPS23754. They needed a 24V output solution. We gave them TI's TPS23754_EVM420_24V_TestReport.pdf reference design to copy.
They have been drawing up the schematic for the TPS23754 with a 24V output. Looking over the adapter input section they have a question. They have gone through the equations for choosing the correct values of R17, R18, and R19 (under the PPD and APD sections) in the attached image of the schematic. They double checked that these values will work for a 12V – 24V adapter input. The PPD and APD have threshold voltages in order to enable them, however, it doesn’t appear that the given equations will meet these thresholds. Is this because the VSS and SGND are at different potentials?
Can you answer this question please?
Thanks for your help.
Regards,
WH