How does the ICUT current limit encoder (table 15) of TPS23861 datasheet relate to the different POE classes. I am looking at adding class protection so that a class 1 device is unable to pull more than its class current. as i understand class 1 can supply up to 4W from the PSE, The spec voltage range at PSE is 44 - 57V (im using 48V) this means that class one can pull 70mA to 90mA which is not an option in the table.
Thank for your help.