Other Parts Discussed in Thread: TPS23861, TPS2388
Hi Sir,
Our client meets the detection issue of PSE controller TPS2384 and could be duplicated in TPS2384EVM.
And they found the Cgood cap(0.22uF) of EVM is over the 802.3at specification max.(0.15uF), and remove the Cgood(C1A1) cap then test it again the result is work normally.
So there are two questions need your help:
1. What TI consideration to design 0.22uF in Cgood(C1A1)?
2. Is there any compatibility issue related to TPS2384?
Thanks
Regards,
Ken