Hello,
Customer notice that there is a residual voltage measured on the MOSFET source terminal when it is turned OFF and the amplitude increased over temperature as table shown below.
Below is customer's circuit, the Gate-Source terminal is connected with a 10M resistor, during OFF state the Gate terminal is grounded with a 2K resistor. The Drain is connected to a 8V battery, the Source pin of MOSFET is connected to system side.
May we know at what temperature would the MOSFET VDS completely breakdown? Please advise
Application: Battery Pack for servo system backup power
Customer: in TW
Discharge MOSFET using CSD17573Q5B
Regards,
Brian