See the title. These pins are designated NC and are on the 4 corners of the device. If these truly need to be NC, what are these pins connected to?
Thanks,
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
See the title. These pins are designated NC and are on the 4 corners of the device. If these truly need to be NC, what are these pins connected to?
Thanks,
David
David,
These pins are not connected to anything internally. They are meant to serve as mechanical "hold downs" to improve board level reliability and can be connected anywhere on the board.
Just note that the bottom pad of the power block is VIN, not PGND.