Hi ,
I am designing a motor driver with mosfets in this regard I am in bit confusion with the below question
1. Why there is max Vgs rating ?
2. Does it indicate the gate oxide breakdown voltage?
3. If the 2 is correct , then the rating should be applicable to the Vgd also .
4. if 3 is correct i.e. the max Vgs applies to Vgd also : then considering a NMOS with gate and source sorted and Vds at its max level, Vgd will be very high compare to max Vgs rating ( max Vds >> max Vgs generally). So for this case also capacitor breakdown is expected.
Thanks is advance .
-biprangshu saha