Dear TI Support,
We need to develop an H Bridge using your components.
The input of the H Bridge will be a regulable 0-48V voltage and two PWM signals created by our microprocessor that interact with a driver like the Infineon IR2110 drive the mosfet of the H Bridge. The H Bridge will be connected in the output with a coil / transformer to generate a sinusoidal high voltage signal (1200V peak to peak. 1200V is the peak to peak voltage of the sinusoidal signal on the second side of the transformer).
The frequency of the sinusoidal signal will be in the tange 100kHz – 3MHz depending the regulation of the two PWM signals, generated by microprocessor, applied to the mosfet of the H bridge.
Eventually we could generate the four signals for the control of the H Bridge instead of using a driver similar to IR2110.
Which components and which solution do you suggest to us?
Let me know!
Best regards