The requirement for output capacitor ESR is confusing us. This is on page 14 of the datasheet. It says the ESR for the electrolytic capacitors can be no lower than 10 mohms (17 m ohms for a single electrolytic capacitor). However, the following paragraph says the ESR is not critical for ceramic capacitors. This is causing our analog experts to still apply the ESR limit to the ceramic capacitors since they say capacitance is capacitance and ESR is ESR whether it is electrolytic or ceramic. But we need more ceramic capacitors for the loads we have. So we are between a rock and a hard place and can't agree how to use the PTN78000HAH.
So why the ESR limit on the electrolytic capacitors when you place no ESR limit on the ceramic capacitors?
Eric