Hello. Team.
I got a question from Our customer Sammy. The question is about the exposed thermal pins (pin#45,46,47)of LMZ31503.
When these pins do not connect with PCB, does LMZ31503 function at all temp(until Ta=85 degC)?
They worry about the case that the solder crack occurred in their field.
Their condition is as follows.
Vin=12V
Vout=3.3V
Iout=2A(max)
And, What percentage does soldered area need it with each pins?
When these pins do not connect with PCB, does theta ja change to around several degC?
Please advise me.
Thanks and Regards,
H.Igari