Hello
I am using PTH12000WAH.
There is a question.
Although it is used on the following conditions,
the temperature of the parts carried in the module has reached 110℃.
Is this OK? In OK, please teach me a reason.
Vin:12V
Vout:5V
Iout:3.25A
Ambient air temperature:40℃
Case temperature of Parts :110℃(Attachment data )
Thank you。