This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78060H The mean of "Vmin" in Rset Formula (1)

Other Parts Discussed in Thread: PTN78060H, PTN78060W

Hi,

Could you tell me the mean of "Vmin" in Rset Formula (1)?
Formula is the folloing.
Rset = 54.9k-ohm * 1.25V / (Vo - Vmin) -Rp

Table 1 shows that Vmin is 2.5.
But I use PTN78060H by 28Vin.
I think that this value is 2.8(0.1 * Vin) if Vin shows Vo adj min.
Which is correct? Is Vmin 2.5V or 2.8V? when PTN78060H is used by 28Vin.

Regards,
Shimizu