Hello I am thinking of using the TPS84410 in the following scenario.
Vin = 3.3V +/- 5%
Vout = 1.8V
load= up to 4A
The 3.3V is coming from a switched supply on another PCB and it will be noisy. My concern is the UVLO. The data sheet indicates that Vin can go down to 2.95V, but the data sheet also indicates the UVLO can have a maximum of 3.135V. These seem to be opposing parameters. How can Vin min be 2.95 if the worst case UVLO is 3.135V (with a hysteresis of 300mV).
Regards,
Guy