Please let me know about internal function of DCR010505 below.
①Is there detailed information of internal LDO regulator?
Customer request is confirm the operation of Vin:6V and 3.3V condition.
I think that if LDO regulator function is clear, these are clear,too.
②On the external sync, why fsw is limited to only 800kHz (±10%)?
③Is there input consumption current on EN:Low condition?
I think that Enable is control LDO regulator only, DC/DC is always moving, is it correct?
Best regards,
Satoshi